This folder contains supporting documents and files for the MiniZed Streaming
I/O SDSoC platform.  The following list describes the contents.

board_def               - Directory containing MiniZed board defintion files
platforms               - Directory containing pre-built MiniZed stream I/O SDSoC platform
sd_card                 - Pre-built application
source                  - Directory containing source code for the SDSoC application
axi_counter_ip.zip      - Zip-file containing an AXI Counter IP
create_mz_stream_bd.tcl - Tcl file that can be used to create the block design
mz_stream_pfm.tcl       - Tcl script used to define platform interfaces available to the SDSoC application
README.txt              - This file.