Article

Agentic AI for embedded control architectures

Avnet A Frame
industrial control panel with agentic AI overlay
Agentic AI is being added to industrial control architectures, showing how new technologies can help improve existing solutions
KEY TAKEAWAYS:
  • Agentic AI can tune set points or suggest actions, but needs limits, watchdogs and fallback behavior.
  • Choose the control architecture to match the risk and complexity.
  • Partition hardware by timing criticality, to maintain real-time when latency isn’t an option.

Agentic AI is appearing in real systems: spinning motors, opening valves and keeping vehicles on course. Design teams need practical ways to add these capabilities without losing the predictability of classical control.

Three common control-loop architectures combine deterministic control with agentic functions in MCUs and MPUs. Avnet can help teams evaluate, prototype and scale these patterns in real deployments, like industrial drives and mobile robots.

Why combine agentic AI with deterministic control architectures?

Classical control algorithms such as Proportional-Integral-Derivative (PID) controllers have decades of operational history in factory drives, power systems and robots, so engineers know how to tune, validate and certify them. Agentic approaches add software components that can set goals, plan actions, call machine learning models and adapt to changing conditions over time. The practical opportunity is to let the agent optimize and adapt while a deterministic layer enforces hard limits on what the agent can command.

In an industrial drive or autonomous mobile robot, that means keeping torque, speed and position inside safe bounds while still reacting to changing workloads, routes or energy targets. The deterministic layer is the guardrail; the agent adds flexibility inside those guardrails.

In practice, control engineers experiment with many ways to pair agentic functions with deterministic loops. Three architectures appear frequently in industrial drives and mobile robotics:

  • A classic PID loop with an agent that tunes set points.
  • A supervisory agent that switches between certified modes.
  • An AI advisor running on an accelerator while deterministic control retains final authority.

Architecture 1: PID control loop with a set-point tuning agent

The first architecture keeps the core loop completely classical. A PID controller runs at a fixed, relatively high frequency on the MCU or drive-control core, while an agentic component works more slowly in the background to adjust set points or tuning parameters. In a motor drive, the agent may monitor energy use, temperature and production targets, then adjust speed references, ramp rates or gains within strict limits.

In a mobile robot, the inner loop can keep wheel velocity stable while the agent adjusts maximum speed or acceleration based on battery state or congestion. This model works because the deterministic loop retains full authority and every change passes through explicit checks before it reaches the controller.

Safety guardrails for PID plus agent

  • Clamp every agent-generated parameter to allowable ranges.
  • Rate-limit changes to speed reference or controller gains so transitions stay smooth.
  • Use watchdog timers so the PID loop keeps running if the agent stalls or misbehaves.
  • Log all parameter updates for traceability.

The agent can run on a second core in a dual-core MCU, on a small application processor linked to a real-time control unit or on an NPU whose outputs are wrapped in deterministic limit-enforcement logic.

Architecture 2: Supervisory AI agent managing certified operating modes

The second architecture places a supervisory agent above several pre-certified deterministic modes such as high-efficiency, high-performance, safe-halt or maintenance mode. In this design, the agent does not shape individual control signals; it decides when to switch between validated modes using context such as production schedules, grid-price signals, predicted wear or user priorities.

In a mobile robot, those modes might include indoor navigation, outdoor rough-terrain travel, docking and emergency stop. This gives teams a middle ground: the system adapts at a higher level, but the building blocks remain deterministic and testable.

Safety guardrails for supervisory mode control

  • Define each mode with clear entry conditions, exit conditions and safe transitions.
  • Let the agent request a mode change, but require a deterministic layer to validate it.
  • Define fallback behavior for missing data or faults in every mode.
  • Use hardware or low-level software watchdogs to force a safe mode if the agent crashes or issues inconsistent requests.

Typically, the deterministic modes run on the MCU or dedicated drive controller, while the agent can run on an MPU, a system-on-module or even in the cloud if latency and fail-safe behavior are acceptable.

Architecture 3: AI advisor on an accelerator with deterministic actuation

The third architecture uses an accelerator, such as an NPU, as an advisor that suggests control actions while a deterministic loop on the MCU or MPU remains responsible for final actuation. In an industrial drive, the advisor may predict load changes or detect anomalies in vibration patterns; in a mobile robot, it may suggest trajectories, obstacle-avoidance moves or battery-management strategies. The deterministic layer checks every suggestion against safety and comfort constraints before applying it.

This architecture enables richer capabilities, but only if the deterministic layer remains the final authority.

Safety guardrails for AI advisor architectures

  • Treat advisor outputs as recommendations, not commands
  • Validate each recommendation against acceleration, jerk, safety-distance or other application limits.
  • Combine confidence scores from machine learning models with rule-based logic so low-confidence outputs trigger conservative behavior.
  • Fall back to simpler control or predefined behaviors if the advisor is unavailable or uncertain.

The real-time loop should run at a fixed rate and use advisor outputs only when they are ready and valid, and safety-critical signals should never depend solely on the advisor.

Embedded AI control architectures overview

Architecture Core idea Agent role Deterministic role Best suited for
PID with set-point tuning agent Classic proportional-integral-derivative loop stays in charge Adjusts set points and tuning within limits Runs real-time loop, enforces bounds and watchdogs Incremental upgrades to existing drives and basic robots
Supervisory agent with certified modes Several pre-validated operating modes Chooses and schedules modes based on context Executes modes, controls transitions, handles safe states Safety-critical drives, elevators, cranes, conveyors
AI advisor with deterministic actuation Learning system recommends actions Provides predictions and trajectory or setting suggestions Validates recommendations, applies only safe commands

Predictive maintenance, advanced robotics, adaptive motion

How to partition AI, control and hardware resources

In all three architectures, sensor interfaces, time-critical loops and actuator control should stay on the MCU or other dedicated control hardware to keep latency low and timing predictable. The agent or advisor can run on a higher-performance core in the same device, on a companion MPU running Linux or an RTOS, or on a dedicated accelerator for machine-learning inference. Engineers should map which tasks need hard real-time response, which can tolerate latency and jitter, and what bandwidth is available between processing elements.

Security also matters. Agents connected to higher-level systems or cloud services should authenticate updates, protect data in transit and fail safely if communication is lost or compromised.

Industrial drives and mobile robots

Industrial drives are a strong testbed for these patterns because they already have well-understood control loops, established safety mechanisms and rich telemetry. A drive designer can begin with set-point tuning to reduce energy use, move to supervisory control to coordinate several drives and then add advisor functions for predictive maintenance based on vibration and temperature data.

Mobile robots add more degrees of freedom and more environmental uncertainty, which makes agentic designs attractive but harder to validate. A small warehouse robot might start with set-point tuning, grow into supervisory coordination across operating modes and eventually use an advisor for path planning while a deterministic motion controller enforces kinematic limits and safe distances.

Ecosystem trends in edge AI for control architectures

These architectures depend on more than algorithms. They also rely on tools for data collection, model training, deployment, observability and lifecycle management, and industry ecosystems help teams share reference designs, safety practices and deployment architectures instead of starting from scratch.

The Edge AI Foundation provides working groups, shared resources and a neutral forum for advancing efficient, scalable edge AI in production settings. As a foundation supporter partner, Avnet is helping to connect embedded hardware, software ecosystems and deployment pathways, while related community efforts and hands-on programs lower the barrier to evaluating and prototyping new edge AI patterns.

Practical steps to start an agentic AI control architecture project

For a first project, teams can take a staged path:

  1. Instrument an existing control loop and gather performance data.
  2. Prototype an offline agent that analyzes the data and proposes set-point or mode changes without yet closing the loop.
  3. Implement the simplest architecture, usually set-point tuning, with strict clamping and logging.
  4. Evaluate behavior under edge cases and faults before moving to supervisory or advisory features.

By treating agentic capabilities as an added layer rather than a replacement for deterministic control, teams can move toward more intelligent drives and robots while retaining the predictability their applications demand.

About Author

Avnet A Frame
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Helpful Links

Marketing Content Spots

Related Articles

Related Articles
AI at the Edge Goes to Work
2027 outlook: AI is expanding to the edge, where intelligence goes to work
By Matt Weldon   -   November 9, 2026
Discover how Avnet Integrated Solutions enables edge AI across industries—helping companies design, build, deploy and support intelligent solutions where real-time decisions matter most.
Digital bar chart rising from a semiconductor chip on a circuit board, representing growth in AI and semiconductor markets.
The Next Wave of AI: Building for the Edge in a Changing Semiconductor Market
By Alex Iuorio   -   July 21, 2026
Edge AI is entering its next growth phase, creating new opportunities for embedded innovation while increasing the importance of supply-chain planning, component strategy, manufacturability, and long-term product support.

Related Events

Related Events
What, Why & How of Vision AI at the Edge
Date: April 23, 2021
Location: On Demand

agentic-ai-for-embedded-control-architectures