Article

Batteries are key to charging options

Electronic circuit board

Wired power is a strong option for developers that need to get to market fast and require an inexpensive, proven solution. For products where convenience and future compatibility are paramount, you can move forward confidently with standards-based wireless power. However, whether you are ditching cords for coils and diving into the $22 billion wireless charging industry or taking advantage of the tried and true wired method, one thing is for certain: it all comes down to the battery.

Making sure the battery matches the charging option, no matter if it’s the next great AI robot or a full industrial IoT deployment, is key to a product’s success.

Application can dictate battery, charging types

Countless battery types have emerged over the years. Lead acid technology dates back to the 1800s, yet it’s still used heavily in automotive and solar applications—so you’ll likely not come across it while researching applicable options for an instrument or wearable.

Nickel-metal hydride technology came along in the late ‘60s and remains a popular choice for consumer electronics and electric vehicles so it might be nice to consider.

However, for portable applications, these batteries are increasingly being eclipsed by lithium-ion, which offers superior power density and faster charging—at a higher price that’s usually worth paying. Lithium-ion batteries are common in consumer electronics and are gaining popularity in automotive and aerospace applications.

Which of these batteries is right for you? You’ll need to balance size and weight with cost, capabilities, and safety. Here are a few important characteristics that you should consider when exploring battery options.

Battery topologies important for powering devices

Get comfortable with two phrases: battery gauging and cell balancing. Battery gauging refers to a battery's ability to accurately assess and report its energy levels. This is an essential feature for most consumer electronics applications. Cell balancing is crucial to maximizing the capacity and extending the life of a battery. These attributes can greatly impact a user's experience of your product.

Battery configurations, also known as topologies, can have a big impact on the complexity and costs of your designs as well. These span centralized, distributed and modular:

  • Centralized topologies employ a single controller connected to multiple battery cells, each with its own communication wire. It's an economical approach that is a good choice for most consumer electronics products such wearables, connected home sensors, and even drones.
  • Distributed topologies feature separate controllers for each battery cell. This is the most expensive option but also the easiest to install, and most expandable.
  • Modular topologies provide a compromise between the centralized and distributed configurations – they use several controllers, each connected to a small number of cells. These topologies are most often used in products that require networks of batteries, like electric cars.

Consider all the options when designing new products

Understanding the pros and cons of each charging and battery option is key to realizing the full potential of your new product. To learn more about how startups can vet which options are right for your project, check out our communities, Hackster.io and element14. 

Marketing Content Spots

Related Articles

Related Articles
A wireframe of an electric car showing the battery and key electrical components
How the EV drivetrain is moving toward function consolidation
By Avnet Staff   -   September 23, 2026
EVs present new opportunities for function consolidation, delivering lower cost and weight, and simpler wiring. But the shift comes with challenges when combining power, control and safety in a single platform. NXP is leading the evolution.
A printed circuit board showing power components
Six capacitor design takeaways for power supply engineers
By Avnet Staff   -   September 22, 2026
Power supplies are found in almost every electronic design, yet each one has different characteristics. Passive components may appear consistent, but their behavior changes with the application, too. Here’s how.

Related Events

Related Events

No related events found

Batteries are Key to Charging Options