Article

How N&C engineers can manage 7 top AI challenges

Avnet A Frame
7 things N&C engineers worry about in the AI era

AI-era networks are moving faster, their data denser, and their traffic flowing in more directions than ever before — and even tiny inefficiencies can amplify into system-wide slowdowns. This article describes the  seven key impacts of AI on  how modern fabrics are built, upgraded and maintained. Networking and communications engineers who anticipate these challenges are better positioned to tackle them before they slow the system down.
 

1. East-west bandwidth that grows overnight

It’s no secret that traffic isn’t just north–south anymore. But the shift to GPU-driven, model-parallel workloads has turned “a little more east–west” into a full-blown surge. Data that used to trickle between racks now floods the spine every time a training cycle spins up. Even well-balanced fabrics can saturate faster than monitoring tools can catch it.

Why it matters: The architecture didn’t break—your workload pattern did. When internal traffic doubles without warning, delay costs and utilization losses start to look the same on the balance sheet.

Engineer mindset: Watch for silent saturation between spine layers, model actual burst loads, and treat optics lead-time like a design constraint.
 

2. Tail latency that refuses to hide

You already track latency, but AI workloads expose a different problem — it’s not the average that has the most impact, it’s the outliers. In multi-node training or inference, a single straggling packet can stall an entire synchronization cycle. The mean may look fine, but the model still waits.

Why it matters: Tail latency is the new system bottleneck. It’s amplified by microbursts, uneven queue discipline and flow-control edge cases that traditional monitoring often misses. Those rare spikes define the true throughput, not the average.

Engineer mindset: Measure beyond P99, not just P95. Correlate queue depth, buffer utilization and fabric congestion with job-completion metrics — that’s where the real inefficiencies hide.
 

3. Observability that drifts out of reach

Do you have too much monitoring? Probably. But as AI clusters rapidly expand and fabrics grow denser, telemetry that used to be clear has turned noisy and fragmented. Every new layer of visibility adds integration debt, and by the time dashboards stabilize, the topology has often Already changed.

Why it matters: Partial visibility can breed false confidence. When path metrics, queue stats, and GPU job telemetry don’t align, it’s increasingly likely you’ll miss real choke points — and you’re not alone. According to Edge Delta’s 2023 report, Charting Observability, 84 percent of organizations report struggling with observability due to tool sprawl, data volume, and rising costs. A provider of a collaborative multi-agent platform for real-time data streaming, Edge Delta based this report on interviews with 200 DevOps and SRE professionals. 

Bottom line: That’s how teams waste hours tuning the wrong layer.

Engineer mindset: Consolidate around golden metrics — latency variance, buffer occupancy and packet-loss correlation to compute delay. Instrument once, validate often, and automate the baseline so it evolves with the network, not behind it.
 

4. Lead-time versus idle-GPU cost

Supply realities don’t always cooperate with your months-out capacity plans. Optics, switches, and cables arrive in staggered batches, while your GPUs sit powered off, waiting to begin work. In fact, studies show many large-scale GPU clusters operate at 50% or less utilization, and dedicated clusters often require ~33% utilization just to be cost-effective. When networking delays push your compute line idle, the ROI vanishes fast.

Engineer mindset: Model supply-chain and lead-time risk like any other infrastructure constraint. Track historical delivery data, quantify the idle-GPU cost model for your cluster, and include it in architecture reviews before gear ships.

Why it matters: Lead-time risk isn’t theoretical—it’s operational. Networking delays stall compute ramp-up, inflate TCO and scramble project timelines. When the fabric isn’t ready, every day of idle hardware compounds loss and erodes confidence in delivery forecasts. That’s why lead-time management now sits alongside power, cooling, and compliance as a core design variable.

Engineer mindset: Model supply volatility the same way you model power or cooling. Track historical delivery lead times and include “delay cost per rack” in design reviews so stakeholders see the impact early — before it hits the balance sheet.
 

5. Upgrade windows without brownouts

The maintenance window isn’t what it used to be. With AI clusters running around the clock and tenants expecting zero interruption, even a minor firmware patch can feel like open-heart surgery. The fabric’s density, traffic mix and automation layers make every upgrade feel like a live-fire event.

Why it matters: Rolling upgrades now carry real business exposure. A single mistimed firmware push or buffer mis-tune can take out multiple training jobs or tenant sessions in seconds. Network stability, once a background concern, has become a key performance indicator. The refresh cycle hasn’t slowed—but the tolerance for downtime has vanished.

Engineer mindset: Treat upgrade planning like workload orchestration: blue-green segments, staged firmware testing, and rollback automation are table stakes. Maintain golden images for every switch family and track mean-time-to-rollback as carefully as mean-time-to-repair.
 

6. Isolation that’s visible, not assumed

You build for separation—VLANs, VRFs, ACLs—but today’s multi-tenant and multi-workload environments demand more than configuration boundaries. As clusters stretch across clouds, and workloads mix AI training with production inference, isolation has to be provable and secure.

Why it matters: It’s no longer enough to assume segmentation works; you have to see it. Yet 35 % of teams admit they still lack visibility into full network paths—including cloud and internet segments.2 That blind spot turns every new tenant or microservice into a potential cross-talk risk. In high-value AI workloads, a single leak or misrouted flow can breach data boundaries or destroy confidence in shared infrastructure.

Engineer mindset: Build isolation you can validate. Use synthetic probes, policy-as-code enforcement, and continuous verification pipelines to prove segmentation holds under load. Correlate telemetry from on-prem and cloud fabrics so visibility doesn’t end at the VPN or gateway.
 

7. Compliance built in, not bolted on

Teams can treat compliance like an inspection—something tacked on at the end that demands paperwork. But as regulations tighten across data residency, export controls, and safety standards, compliance increasingly needs to be built into the design itself. New deployments, whether in a hazardous zone or across borders, bring their own checklist of certifications, housing requirements, and data-handling rules.

Why it matters: Waiting until the audit to verify compliance is too late. Every missed requirement—NEBS for telecom, FIPS/NIST for encryption, export-control documentation—can delay activation or trigger costly retrofits. Building with these frameworks in mind shortens approval cycles and reduces rework risk.

Engineer mindset: Design with compliance as a design constraint, not a phase-two task. Maintain living documentation, validated component libraries, and automated checks for region-specific standards. When compliance data is tied directly to your bill of materials and configuration templates, it becomes an enabler rather than a drag on delivery.
 

Conclusion

Modern Networking and Communications engineers don’t have to react to change, they can anticipate it. The shift to AI-era workloads has exposed the fabric’s hidden dependencies: bandwidth patterns, latency spikes, observability gaps, supply volatility, upgrade risk, isolation, and compliance. Each of these pressures is familiar on its own, but together they define a new operational baseline—one where timing, visibility, and validation matter as much as raw throughput.

Forward-thinking engineers who recognize these trends keep systems stable and business goals intact. That’s the difference between reactive maintenance and strategic readiness.

If these challenges sound familiar, you’re not alone. And you have a path forward. The next step is translating what you know into a decision-making framework—when to build, when to buy, and when to blend both.

About Author

Avnet A Frame
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Marketing Content Spots

Related Articles

Related Articles
A wirelessly connected battery-powered industrial sensor sits on top of an electric motor housing.
Rethinking RF and analog front ends for smarter edge AI
By Avnet Staff   -   July 2, 2026
This article treats RF and AI as one design problem, exploring how to partition RF/AFE, data conversion and edge processing across vibration, RF condition monitoring and low power sensing use cases, with a practical co design checklist.
A base station in an industrial setting with a digital twin represented alongside
Using digital twins for hardware component selection
By Avnet Staff   -   July 1, 2026
Engineers may be leaving too much design intelligence on the table by not using digital twins to their fullest potential. More manufacturers are now providing models that can be used to evaluate design options earlier in the process.

Related Events

Related Events
satellite in orbit
Space 2.0: AMD Technologies for New Space
Date: February 23, 2022
Location: Webinar

how-n-and-c-engineers-can-manage-7-top-ai-challenges