Article

Power, Thermal, and Compute Constraints

Avnet A Frame
Thermal imaging camera measuring heat on an electronic circuit board.
Designing for sustained performance, not peak benchmarks.

Overview

As AI inference moves into battery-powered devices, industrial equipment, robotics, medical systems, and intelligent sensors, engineering teams face a growing challenge: delivering more intelligence within fixed power and thermal constraints.

Running AI at the edge is no longer simply a question of whether a model can execute on a device. The more difficult challenge is ensuring that the system can sustain the required performance while operating within the power budget and thermal limits of the target application. Designs that overlook these constraints often encounter shortened battery life, thermal throttling, reduced reliability, or costly late-stage redesigns.

The central task is balancing processing performance against energy consumption and heat dissipation from the earliest architecture decisions. As Edge AI moves from experimentation into deployed products, success increasingly depends on how effectively engineers manage this balance.

Recent findings from Avnet Insights: The Reality of Artificial Intelligence reflect this reality. As AI becomes part of production systems, power requirements and temperature regulation rank among the most frequently cited design challenges, while sustainability concerns continue to grow alongside the increased energy demands of AI-enabled devices.
 

The challenge: matching silicon to a power and thermal budget

Selecting the right silicon for an Edge AI application is increasingly complex. Available hardware spans a broad spectrum, including CPUs, GPUs, FPGAs, and dedicated neural processing units (NPUs), each offering a different balance of performance, power consumption, and thermal characteristics.

At the general-purpose end are MCUs, MPUs, and CPUs. Many of these devices integrate or support additional acceleration through GPUs, FPGAs, or NPUs. The resulting combinations give engineers tremendous flexibility but also create difficult tradeoffs between compute capability, power efficiency, and thermal management.

Four fundamental questions shape every Edge AI hardware decision:

  • What is the application expected to accomplish?
  • What level of inference performance is required?
  • What power budget is available?
  • What thermal solution is practical within the target enclosure?
     

These questions cannot be evaluated independently. Improvements in performance often increase power consumption and heat generation. Optimizing one dimension frequently affects the others. Understanding these relationships is critical to designing systems that succeed outside the lab and in real-world deployment environments.
 

Why this is difficult

Many Edge AI challenges stem from how hardware performance is measured and presented. Specifications provide valuable information, but different vendors often report metrics using different workloads, measurement boundaries, and operating conditions.

Understanding the context behind those numbers is just as important as understanding the numbers themselves.
 

Compute performance requires context

Several metrics are commonly used to describe AI processing capability:

  • TOPS (tera-operations per second)
  • FPS (frames per second)
  • Latency
     

FPS and latency reflect performance for a specific workload and therefore provide useful comparisons when measured consistently.

TOPS is often used as a shorthand measure of AI performance, but multiple versions exist:

  • Sparse TOPS
  • Dense TOPS
  • Effective TOPS
     

Sparse TOPS may count operations that are skipped during execution because of model sparsity, producing figures that appear significantly higher than actual computational work performed. Dense TOPS represents theoretical performance under ideal conditions.

However, Edge AI systems are rarely limited by compute alone. Data movement, memory bandwidth, and movement of model weights frequently become bottlenecks that prevent hardware from reaching theoretical peak performance. Effective TOPS attempts to account for these practical limitations.
 

A useful rule of thumb is:

Sparse TOPS > Dense TOPS > Effective TOPS

For many real-world applications, Effective TOPS often provides the most meaningful representation of achievable performance.
 

Power efficiency determines practical deployment

A second group of metrics describes how efficiently a device performs useful work:

  • FPS/W (frames per second per watt)
  • J/frame (joules per frame)
  • TOPS/W (tera-operations per second per watt)

These measurements become particularly important in battery-powered, fanless, and thermally constrained systems.

Like compute metrics, power measurements depend heavily on what was included in the test. Published values frequently represent the silicon device itself and may exclude external memory, interface circuitry, or other system-level components.

As a result, two devices may appear similar on paper while exhibiting significantly different real-world power consumption once integrated into a complete system.
 

Thermal constraints often define the system

Of the three design considerations, thermal behavior is often the most difficult to evaluate and the most likely to impact long-term performance.

Most published benchmark results are generated before a device reaches steady-state operating temperature. However, deployed systems must operate continuously under actual environmental conditions.

Two questions therefore become critical:

  • How does performance change once the system reaches a stable operating temperature?
  • How does performance change when airflow is limited or unavailable?
     

When thermal dissipation is insufficient, devices enter thermal throttling to protect themselves from damage. Performance that appears achievable during initial testing may not be sustainable in a compact enclosure, sealed industrial environment, or battery-powered product.

In many Edge AI deployments, thermal design ultimately becomes the limiting factor. A platform may have sufficient compute capability on paper but fail to sustain that performance under real operating conditions.

For this reason engineers should perform thermal validation using the intended enclosure, workload, and duty cycle whenever possible.
 

Understanding what was measured

Every device has operating conditions under which it performs best, and performance specifications naturally emphasize those conditions.

The engineering challenge is not determining whether published metrics are accurate. It is determining what they actually represent.

Engineers should evaluate:

  • Which workload was measured
  • What system components were included
  • Whether results reflect peak or sustained performance
  • The thermal conditions present during testing
     

Viewed through this lens, hardware comparisons become far more meaningful and directly relevant to real-world system requirements.
 

Addressing power, thermal, and compute constraints

Successful Edge AI systems approach power, thermal, and compute considerations as a single engineering problem rather than three separate specifications.

The process begins by defining:

  • Application requirements
  • Throughput and latency goals
  • Available power budget
  • Thermal conditions of the target environment

These factors should guide hardware selection before individual devices are evaluated.

Engineers should interpret vendor metrics within the context of how vendors measured them. Comparing devices using consistent assumptions around workloads, power boundaries, and thermal conditions generally provides more useful insight than comparing headline performance claims alone.

Most importantly, candidate architectures should be validated under realistic operating conditions. Real workloads, real enclosures, and sustained operating temperatures frequently reveal limitations that benchmark specifications cannot predict.

The most successful Edge AI deployments balance performance, energy consumption, memory requirements, and thermal behavior as a complete system rather than optimizing any single metric in isolation.
 

Accelerating design validation

Engineering support can help reduce the risk associated with power and thermal decisions made early in the design cycle.

Areas where design assistance can be valuable include:

  • Selecting processors, SoCs, and accelerators aligned to workload requirements
  • Performing thermal simulation and enclosure analysis
  • Evaluating passive cooling approaches
  • Validating performance under real operating conditions
  • Reviewing designs for manufacturability and long-term reliability
     

Early validation often identifies issues that would otherwise appear much later in development, when corrective action becomes significantly more costly.
 

Designing for sustained performance

Successful Edge AI designs are rarely constrained by compute capability alone. More often, power delivery, memory movement, and thermal dissipation determine whether a system can sustain its intended performance over time.

Engineering teams that evaluate compute, power, and thermal requirements as a unified budget are better positioned to avoid redesigns, achieve predictable performance, and deploy reliable products at scale.

The question is not whether a device can achieve peak AI performance under ideal conditions. The real challenge is whether it can deliver the required performance consistently, efficiently, and reliably within the constraints of the final product. That distinction often determines whether an Edge AI concept becomes a successful production system.

 

About Author

Avnet A Frame
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Marketing Content Spots

Related Articles

Related Articles
AI at the Edge Goes to Work
2027 outlook: AI is expanding to the edge, where intelligence goes to work
By Matt Weldon   -   November 9, 2026
Discover how Avnet Integrated Solutions enables edge AI across industries—helping companies design, build, deploy and support intelligent solutions where real-time decisions matter most.
An electric scooter highlighting the critical electronic subsystems
Targeted solutions for e-mobility’s five critical subsystems
By Avnet Staff   -   September 28, 2026
From efficient power conversion to connected rider experiences, bringing semiconductors, software, reference designs and system-level platforms together is accelerating e-mobility development.

Related Events

Related Events
airplane cockpit looking out on the runway
More Electrification in Aircraft
Date: October 11, 2022
Location: Virtual
What, Why & How of Vision AI at the Edge
Date: April 23, 2021
Location: On Demand

power-thermal-and-compute-constraints