ai-based-image-recognition-does-the-hard-work

ai-based-image-recognition-does-the-hard-work

AI-based image recognition does the hard work

Philip Ling
Facial recognition auitomotive camera

It takes time to look at an image and decide on an action. Machines look at digital images much faster than people, but they need to understand the content. Artificial intelligence (AI) is making that possible.

Computer vision is a big topic. Image recognition restricts itself to detecting objects in a still image or a frame in a video. Objects are real, like a bottle or a dog, rather than abstract, like bad weather or danger. Detecting real objects is relatively simple and although AI has limitations, object detection and classification is quick and accurate.

You already use AI

It isn’t always obvious when you are using AI. It is now a mature technology used by large organizations everywhere. Some examples of how we use AI-based image recognition in everyday life include: 

  • Social media companies use image recognition to audibly describe what is in a picture to visually impaired users.
  • Search engines use images to identify objects and locations, such as bridges.
  • Apps use images instead of text to search for products, retailers and brands.

But AI isn’t limited to large organizations with deep pockets and big databases. Any IoT application can use AI and machine learning to add useful features.

How AI makes IoT better

Reducing human effort is one of the main values of AI. Identifying objects in images requires a lot of mental acuity. AI-based image recognition is relieving user effort and increasing productivity in these ways:

  • defect detection
  • quality checks
  • alignment
  • assembly
  • welding
The 8 stages of image recognition using artificial intelligence

 

AI visually inspects work areas or equipment to check safety or for damage. Heavy industries use image recognition to detect machine wear. It also sees corrosion on infrastructure like pipes, storage tanks and even vehicles.

Using image recognition creates a history of detail. Stored images get tagged with the date, location and status. AI analyzes the database to predict maintenance or replacement.

Example chart of AI-based image recognitionExample applications for AI-based image recognition

 

Object detection in vertical industries

Using AI to detect objects in images is possible in all vertical industries. These expert systems can increase throughput in high-volume, cost-sensitive industries. They can also increase reliability in safety-critical applications.

Here are some specific examples of how industries are using AI:

Oil and Gas

Geology: Oil and gas companies employ experts to analyze locations. They use their expertise to estimate the deposit of fossil fuels. AI helps geoscientists during the exploration and bore phases by identifying rock compositions.
Maintenance: Mechanical parts like drills wear out quickly in this industry. AI detects wear and predicts when a part may need replacing.
Detection: Oil and gas companies use AI on rigs to monitor the area. Any spills, slicks or leaks are detected quickly and reported automatically. 

Retail

Auditing: Product presentation affects buyer habits. AI monitors these habits and correlates them against product placements. This helps retailers present their products in the best way for the customer.
Inventory: An empty shelf is a lost sale. Image systems monitor stock levels on shelves. Refills are triggered automatically when stock levels are low.

Point of sale: Automatic check-out systems are popular because customers like them. AI-based image recognition detects what’s in the basket. Detecting many items at once makes the process quicker.

Agriculture

Monitoring: Farmers use AI to monitor their crops, soil and growing environment.

Detection: AI detects weeds, unhealthy plants, or insects that may damage the crops.

Yield: Farmers increase their yield using AI. Detecting diseased plants early can stop the spread and protect the crop.

Manufacturing

Quality: AI-based machine vision checks the assembly line. Image recognition assures the quality of components before they enter the production process. 

Assets: AI-based image recognition identifies assets and logs their location.

All these examples are applications built to provide AI-based image recognition. Avnet can help you develop your application and add the power of AI to your IoT solution. Contact us today to discuss how.


 

關於作者

Philip Ling
Philip Ling

Philip Ling is a Technical Content Manager with Avnet. He holds a post-graduate diploma in Advanced ...

ai-based-image-recognition-does-the-hard-work

ai-based-image-recognition-does-the-hard-work

相關文章
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
從輔助工具到即時協作者,AI 超音波設備開啟端側智慧新典範
2026年11月2日
安富利將繼續攜手生態系合作夥伴,推動 AI 從「輔助工具」進化為不可或缺的「即時協作者」,讓優質醫療資源更均衡、更高效地服務每一位患者。
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
當 AI 叢集邁向 1.6T:別只看 GPU,IP&E 才是資料中心的「隱形匯流排」
2026年10月1日
運算晶片定義了效能的「天花板」,IP&E 則決定系統能否在極限負載下穩定運作。從 AEC 銅纜、LPO 光模組,到背板連接器與被動元件,正是 1.6T 時代資料流動的真正基礎。

ai-based-image-recognition-does-the-hard-work

相關活動
Avnet/ Renesas AI webinar
Date: 2020年7月15日
Location: Webinar