the-latest-technologies-driving-home-medical-innovations

the-latest-technologies-driving-home-medical-innovations

The latest technologies driving home medical innovations

Adrien Larevat
man using smartphone and blood monitor
The healthcare industry is under constant pressure to deliver new procedures and treatments against a backdrop of rising costs.

What's Next Magazine

For home-health devices, the patient experience is central to the product. New technologies, including AI, smaller displays with higher pixel density, portable graphic frameworks and more capable MCUs are driving innovation.

The health care industry is under constant pressure to deliver new procedures and treatments against a backdrop of rising costs. Medical breakthroughs only become significant when they can be delivered cost-effectively at scale to the patients who need them.

Semiconductor technology was made to solve problems like this. The evolution of wearable technologies, the emergence of the Internet of Medical Things (IoMT), and more recently the adoption of artificial intelligence (AI) in health care, all rely on new hardware and software, developed for, with and by OEMs working in the medical market.

The three pillars of wearables, IoMT and AI are in convergence. This will see the home health care market grow rapidly in the coming years. Wearables and internet connectivity have been areas of interest for several years, but AI could be the key to unlocking their real potential.

Putting the user first in medical device development

chart

The system integration required for a connected medical device starts with understanding the user and the application, and with keeping patient data secure at every stage. Source: Witekio

Why is AI good for medicine?

It may seem counterintuitive to use a technology infamous for its inaccuracies in an application that so solidly relies on precision. The simple answer is that people are all the same and yet every one of us is different. This juxtaposition between similar and different makes AI a good fit for medical applications.

At a cellular level, humans look the same, but the form those cells take when constructing our features varies massively. The way our organs sit, the way blood flows, the way muscles twitch, these are all biologically similar but visibly dissimilar. Being able to spot small differences in video and images that are ostensibly the same is where AI really excels. Pilot projects show that AI is already as good and sometimes better than trained professionals at detecting cancer cells in breast scans.

Designing medical devices involves a lot of software. That software needs to be compliant with standards that are generally similar around the world but vary by end market. This is where an experienced embedded software partner like Witekio can help.

Witekio is working with the industry’s leading AI hardware platform providers to help medical device manufacturers harness the power of AI. Development starts with robust board support packages (BSPs), developed by Witekio’s engineers for the hardware platform, and moves on to software optimization to manage AI workloads across the hardware resources and through to custom AI model development using the customer’s own data.

Navigating software compliance when developing medical devices

block diagram

Documenting your development journey, recording your test results, and knowing the source of your software are the three universal essentials for compliance when developing medical devices. Source: Witekio

The medical device user experience

An important part of a medical device, particularly one designed to be used outside a medical facility, is the user interface. In fact, the user experience, or UX, should drive the entire product development process.

Graphical user interfaces, or GUIs, are ubiquitous. In some applications, they provide supplementary information or an alternative way to operate a machine. In medical applications, particularly small or wearable devices, a touch-sensitive screen may be the only interface available.

Designing a GUI goes beyond aesthetics. The way information and functions are presented on screen, the way menus intuitively flow, the visual cues and feedback provided—all combine to create a UX that is fundamental to a successful product.

The term “successful” should be interpreted to mean that the patient can operate the device and gain the information they need without constantly consulting a help desk or manual. Medical devices are typically used frequently by a patient. Making them simple but effective is the measure of success. The UX is key.

Witekio’s engineers have accrued hundreds of hours developing GUIs and the UX for all kinds of electronic products, including medical devices and wearables. Witekio recently hosted a webinar, now available on demand, showing GUI development using the Qt graphics framework running on Infineon MCUs.

Part of that demonstration showed a medical device with a graphical representation of a beating heart. As Qt is a cross-platform framework, Witekio was able to show how the application running on a desktop computer can be ported to an embedded platform, such as the Infineon Traveo T2G MCU coupled to a small screen.

Porting a PC GUI to an embedded MCU

block diagram

As a cross-platform graphics framework, Witekio was able to port a medical GUI running on a PC over to an MCU. Source: Witekio

Designing medical products for the home health care market requires specialist knowledge in multiple disciplines. Software development is, itself, multifaceted. It requires an understanding of the application and how medical data is captured, analyzed and actioned. The software must comply with the regulations in the markets where the product will be sold. And the software must deliver the user experience necessary to make the product successful.

Witekio can provide expertise in all these disciplines. With a multinational presence, experienced software engineers, and close working relationships with the semiconductor suppliers OEMs need to work with, Witekio can help take medical products from proof-of-concept to the patient.

 

关于作者

Adrien Larevat
Adrien Larevat

Adrien Leravat is the Solution Director, Embedded Software, at Witekio. Adrien is also an IoT archit...

Helpful Links

the-latest-technologies-driving-home-medical-innovations

the-latest-technologies-driving-home-medical-innovations

相关文章
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
From Assistive Tool to Real-Time Collaborator: AI Ultrasound Ushers in a New Era of Edge Intelligence
2026年11月1日
As AI moves from cloud-based assistance to real-time participation at the edge, it is becoming genuinely embedded in clinical workflows and helping clinicians reduce cognitive burden.
5 men
Roundtable discussion: For today’s supply chain, it’s all about resilience
By Valeri Oliver   -   2025年12月9日
The modern supply chain is always evolving, whether due to geopolitical upheaval, natural disasters or other factors. Hear straight from three of Avnet’s supply chain experts about the latest trends in supply chain resilience, data mapping and more

the-latest-technologies-driving-home-medical-innovations

相关活动

未找到相关活动